I can use a motor profiler with a custom board, but can I use a motor pilot with the same software? Is it possible to use a motor pilot with a custom board?
Is it possible to change the starting direction in open-loop control? Can I adjust the initial parameters based on the potentiometer value? Where can I configure this?
I’m working with the STEVAL-ESC001V1 and noticed that there is no overcurrent protection (OCP) feature. How can I enable or implement OCP using firmware version 6.3.0? Are there any specific guidelines or examples to follow?