User Activity

Hi Folks,This has been driving me crazy. I'm using a Nucleo-L031 board and it's connected to a I2C TCA9548A 1:8 multiplexer. I am trying to read 4 sensors connected to the mux chip. I have 4.7K pullups installed at the Nucleo's I2C pins. The sensor b...
Hi Folks,I have the latest version of the IDE (1.16.1) but now the search feature won't work. It will only return an error:When I try to search for "HAL_StatusTypeDef I2C_WaitOnSTOPFlagUntilTimeout" I get the following set of errors:Text SearchAn int...
Hi Folks,I'm having an issue with just reading and writing new values to the RTC. I'm using a custom board that contains a 32.786Khz crystal and in CubeIDE the LSE is setup properly. I also have a battery connected to Vbatt,I'm using the following to...
Hi Folks,I'm having a problem with connecting my ST-Link/v2 to my new board with a STM32H7ARIT micro on it.I have had no problem connecting the ST-Link to another board with the STM32F103RBT6 micro on it. I have the Debugger configuration in the STM3...
Hi @SofLit,I need to develop a unique serial number for one of our products that will go into production soon. I'd rather use the UID that is built into the STM32H7A3 chip but I have some questions.I understand that it is a 96bit value that I can rea...
Kudos from