User Activity

HelloI have two boards. Both of them are based on STM32 MCUs. One is a SPI master and the second is a SPI slave.Settings for master (STM32H723): mHandle.Init.Mode = SPI_MODE_MASTER; mHandle.Init.Direction ...
Hello guys.I have an interesting project where I need to load user applications (binaries) from external flash memory (FATFS) into RAM and run them from there. Also, I want to use a static library (let's call it libAPI.a for example) that should be a...
Hello guys!In our project we use STM32H750VBT6 MCU and an external NOR-flash chip W25Q128. Tell me please can we use XiP technology and FATFS file system on this flash memory simultaneously? Might there be a conflict at the QSPI level or at the memor...
Kudos from
Kudos given to