User Activity

Device STM32F373CCT648 pin We currently using 2 single ended 16 bit SADC inputs one on SADC1 PE9 and one on SADC2 PB2.We interleave the two 50KHz single channels using a 10uS delay between them. This uses DMA SADC transfer an interleaves the signal t...
Dear community I have purchased a STEVAL STM3201 spin kit,After getting the data sheet for my motor the motor is nearly spinning it is so close.Eventually I will use halls but to walk before I can run I will try sensor-less firstI have used the motor...
Dear CommunityI have developed a BLDC motor drive with a senorles BACKEMF control using a DRV10983 IC.It uses sensor less control no halls used. If I look at the motors hall effects that are not used on the DRV10983 Chip My issue is that the speed is...
Dear communityI have developed a bldc motor driver using a DRV10983 chip from texas instruments target speed 3000.00 RPMIt works of BEMF and dose not use hall effect sensorsI have achieved good stability but the instrument the motor is designed for n...
Kudos from