User Activity

Citing from the STM32L431 manual:The debug pins are in AF pull-up/pull-down after reset:• PA15: JTDI in pull-up• PA14: JTCK/SWCLK in pull-down• PA13: JTMS/SWDAT in pull-up• PB4: NJTRST in pull-up• PB3: JTDO in floating state no pull-up/pull-downLet's...
Hello,Following setup: STM32L431 MCU with 64 pins TQFPThe board I'm using is a minimally soldered version because I could not reach the stated figures in standby mode from the datasheet.Necessary capacitors are soldered + 1x 22uF 0805 + a 32kHz cryst...
Problem description:1-2 bytes in a ~30 byte message (usually at the same spot in the msg) are sometimes missing. Usually it is the 13th byte.If I send shorter msgs via SPI like 10 bytes, the other party receives them correctly.If I wait 50us after pu...
I have multiple boards with a STM32L051 MCU and 2 board revision, A and B.A: no LSE oscillator, LED connected via 550 Ohm resistor, around 20uF capacitance on VCC, radio module solderedB: 6pF 32kHz +-20 ppm oscillator soldered, 9pF load capacitors, a...
Kudos from