STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
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
jvan .1
Associate II
since
2022-11-25
2023-06-14
User statistics
4
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About jvan .1
Options
Report User
User Activity
Posts
Replies
Using St Cube IDE 1.6.0, I create new project for STM32F302C8. When debugging the project i noticed that my HSE crystal is not working (Systick is always 0). The code ends up in an infinite loop which prevents the HSE. Who can help me ??
2022-11-25
/* USER CODE BEGIN Header *//** ****************************************************************************** * @file : main.c * @brief : Main program body **********************************************************************...
Re: Using St Cube IDE 1.6.0, I create new project for STM32F302C8. When debugging the project i noticed that my HSE crystal is not working (Systick is always 0). The code ends up in an infinite loop which prevents the HSE. Who can help me ??
2022-11-25
In addition, it is strange that the same code works on my nucleo dev board.(STM32F302R8) Is my STM32F302C8 on my PCB broken??
Re: Using St Cube IDE 1.6.0, I create new project for STM32F302C8. When debugging the project i noticed that my HSE crystal is not working (Systick is always 0). The code ends up in an infinite loop which prevents the HSE. Who can help me ??
2022-11-25
The systick also does not work with the HSI
Re: Using St Cube IDE 1.6.0, I create new project for STM32F302C8. When debugging the project i noticed that my HSE crystal is not working (Systick is always 0). The code ends up in an infinite loop which prevents the HSE. Who can help me ??
2022-11-25
These are my clock settings