Skip to main content
ck.1
Associate III
Mar 3, 2023 10:54 AM UTC
Solved

IS STM32H750 TFBGA240 PIN TO PIN Compatible to replace with STM32H755 TFBGA240

IS STM32H750 TFBGA240 PIN TO PIN Compatible to replace with STM32H755 TFBGA240

This topic has been closed for replies.
Sarra.SBest answer
ST Employee
Mar 3, 2023 12:49 PM UTC

Hello @ck.1​ 

Yes, STM32H750 and STM32H755 have the same pinout in their TFBGA240 package so u can replace one with other.

However, you should compare the both datasheets to ensure that there are no functional differences

Hope that helps!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Sarra.SBest answer
ST Employee
Mar 3, 2023 12:49 PM UTC

Hello @ck.1​ 

Yes, STM32H750 and STM32H755 have the same pinout in their TFBGA240 package so u can replace one with other.

However, you should compare the both datasheets to ensure that there are no functional differences

Hope that helps!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.