User Activity

Hi SirI used the same e-marker cable that i tested with FUSB307BGEVB.The Ra in the cable can be detected when i used the FUSB307EGEVB but it didn't be detected by the STUSB1602.I tracked the code i found that when cable attached then the register va...
Act as the DFP. I request the PE to send SOP identify request to the UFP after PE received the data it didn't fire the callback function. (I set the breakpoint at fusb305_tcpc_get_message and i see the data received from the DFP is correct.)But when...