Hi Entony,I will need more information about the versions that you are using. ST25NFCTap Android application is made of 3 layers:At the low level, there is the AndroidReaderInterface which creates a generic interface to access to NFC Tag on Android p...
Hi,For my information, what do you plan to use to communicate with the ST25DV Tag? An NFC Reader connected to a PC? A smartphone?The ST25SDK has an API to transmit large about of data (for example 100kB) through ST25DV's FTM. For example, if you inst...
Hi,If my understanding is correct, you have a lighting product that you want to configure through NFC. Do you want to do this configuration through an NFC Reader on PC or through a smartphone?NFC is indeed very well adapted to this kind of configurat...
Hi,I'm jumping in the discussion. I think that the discussion is going to the right direction: I fully agree that NDEF has no added value here and I also agree that it is wise to use multiple area in this use case.You can have a first area where you...