2023-03-21 11:00 PM
Hello,
st25nfcApplication_V3.7.0 is crashing on my Pixel6A (Android13) caused by the following source:
E/AndroidRuntime: FATAL EXCEPTION: AsyncTask #1
Process: com.st.st25nfc.dbg, PID: 1098
java.lang.RuntimeException: An error occurred while executing doInBackground()
at android.os.AsyncTask$4.done(AsyncTask.java:415)
at java.util.concurrent.FutureTask.finishCompletion(FutureTask.java:381)
at java.util.concurrent.FutureTask.setException(FutureTask.java:250)
at java.util.concurrent.FutureTask.run(FutureTask.java:269)
at android.os.AsyncTask$SerialExecutor$1.run(AsyncTask.java:305)
at java.util.concurrent.ThreadPoolExecutor.runWorker(ThreadPoolExecutor.java:1137)
at java.util.concurrent.ThreadPoolExecutor$Worker.run(ThreadPoolExecutor.java:637)
at java.lang.Thread.run(Thread.java:1012)
Caused by: java.lang.SecurityException: Permission Denial: Tag ( ID: 2E D4 4E 50 00 27 02 E0 ) is out of date
at android.nfc.Tag.getTagService(Tag.java:381)
Could this be the the reasion: ???
Catch a SecurityException that was introduced in AOSP commit 113f3a4. It is thrown when an NFC tag is removed.
https://github.com/open-keychain/open-keychain/pull/2804
Does anyone have a solution ?
Solved! Go to Solution.
2024-04-16 5:30 AM
Hi Oliver,
We have same problem on Android 13... Can you help me please with this error: cannot find symbol
androidReaderInterface.setAndroidTag(newAndroidTag);
setAndroidTag is not defined in AndroidReaderInterface class??
2024-04-16 5:47 AM
Hi Entony,
I will need more information about the versions that you are using. ST25NFCTap Android application is made of 3 layers:
The current version of ST25NFCTap application is 3.9.0.
The current version of ST25SDK is 1.10.0.
The current version of AndroidReaderInterface is 1.0.10.
setAndroidTag() is defined in AndroidReaderInterface. Did you successfully add the AndroidReaderInterface's AAR file to your Android Studio project?
2024-04-16 10:48 PM - edited 2024-04-16 10:48 PM
Hi Oliver,
thank you for your answer. You are right, it was a problem with the AndroidReaderInterface AAR file, I had an older version 1.0.8
2024-04-17 1:08 AM
Hi,
I'm glad to see that your issue is now fixed.
Regards