User Activity

I am working on the stm32G0B1KBUX, i am using FDCAN on it. FDCAN is working fine and i can tranmsit and receive messages.The problem arises when i try to erase a page and try to write data in the flash. I have reserved last page for configurations. M...
Hi,I am using STM32G070RB for a modbus based product. The code is complete but i am facing issues that on some of the controller the code does not work and it gets stuck in the HAL_DELAY() function because the systick interrupt are not getting throug...
Hi,I want to use CBOR for my stm32F7. Is there any recomendation by ST for it or any opensource library that can be integrated?
Hi,I have a structure in code with name Config_t, i want to access the size of this struct in my post build command.How can i do that? The Config_t may get change next time so giving a constant size in the post build command is not an option. Thanks
I looked at both the datasheet and Oscillators design document for stm32 controllers. Both suggested the same speed for external Osciallaotrs for stm32F7 controllers that is 4-26 MHz.BUT, in the stm32cubeMx it gives you option to select external HSE ...
Kudos from