User Activity

CubeMX 6.5.0, Cube-AZRTOS-H7 V2.1.0, TouchGFX 4.19.1make a new project , using threadX os, gui using TouchGFX, project error.MX_TouchGFX_Init(), need input VOID *memory_ptr, but empty.do not excute MX_TouchGFX_PreOSInit();do not excute OSWrappers::i...
Now, using Dynamic Graph Widget in Touch 4.15. We only draw 4 lines, but somtimes picture does not smooth.It looks like it blocked somewhere, button action is delayed. At last we find render time become biger as line draws more. hoping for some help...
Touch Designer set pix format as ARGB2222, RGB LCD using LTDC setted pix format as L8. In a simple project ,now it can show correctly. But I imgrate this project with a Touch Designer Demo Project , it can not work correctly. Error show I found uint1...
I want to chang the theme in our device, like windows which has bright or dark theme.How to do?
Now we have a problem, our stm32 device board is delayed.Now we only can develop our UI on touch designer simulator. But we want to test our software of communication layer, using the serial port or TCP/IP port in one computer with the same port in a...
Kudos from