To ensure the CMD files run correctly from your project path, you can use relative paths or double-check the syntax of your commands. If `${project_loc}\CppToC.cmd` is not working, try using the relative path directly if the CMD files are in the same...
The ADC1_IN16 pin at PA12 cannot be configured on the STM32G030K6T6 using STM32CubeIDE without adjusting the sequencer settings in the parameter settings tab. The error message suggests that enabling this pin requires the sequencer to be set to "not ...