User Activity

stm32mp157f, I need to use uart5 to drive an rs485 but the hardware supplied DE pin is already in use.  So I need to configure a different GPIO to use.  If the device tree binding rts-gpios is supported, then the task is simplified. We can modify the...
Processor stm32mp157f, our board design similar to dk2.In my STM32CubeMX generated device tree (dunfell) I have added the following:/* USER CODE BEGIN root */soc {vrefbuf@50025000 {status = "disabled";};};/* USER CODE END root */I have my vref pin co...
As Mickledore is no longer supported (by yocto) when can we expect an updated yocto release from ST for the stm32mp1 series?
I want to regenerate all my files, originally for the stm32mp157cac for the stm32mp157fac, in particular the devtree files.  I suspect that the files are the same but I need verification.  If they are not the same, how do I go about the update (witho...
I am trying to set up 3 ADC.  I set PA4 to ADC1_INP18, PA5 to ADC2_INP19 and PF11 to ADC1_INP2.  Will this be something that works?  I am monitoring 3 lines (none NEED to be fast).I'm not clear on how to set this up.  I am multiplexing several inputs...
Kudos from