User Activity

Hi everyone,Currently, I am working on STM32MP153 mpu. I am building a Linux image using Yocto.In the image, I want to add a Python package (pyarrow).But when I built the Linux image I got the error, Please see the attached image. 
Is there any way to update 4 textarea with a single invalidate call? Or is there any way to add multiple text area in a custom container and update all text area with a single call of invalidate?
 Currently, i am working on TouchGfx.But my code gets stuck in the first execution of MX_TouchGFX_Process.  I use external RAM and Waveshare 7-inch TFT display.@Piranha  Could please help me to resolve the issue?
I want to perform a bulk transfer from the STM32 device to my host device. Is stm32 USB stack support it support.
Hi allCurrently, I am working on a project in which I have to design an application in such a way that it should support DHCP and static IP mode based on user choice. And this would be in FREERTOS. Users can back and forth between static and DHCP mod...
Kudos from