User Activity

Hello everyone, I encountered a problem while debugging my program.CubeIDE Version 1.14 , CubeProgrammer Version 2.9.0, ST-Link Version V2J43S7 The ST-Link/V2 is found. You can erase the Chip (STM32H753BIT6) but can't download the .elf file (CubeProg...
Hello everyone,I encountered a problem while using TouchGFX. I want to use an external Flash which is connected via QUADSPI.The Flash works fine (manually loading and writing some informations into the memory). Block mode, Memory Mapped mode, both do...
Hello everyone,is it possible to use a display that only supports Data enable mode?If yes, how to configurate the LTDC for this mode? I use the STM32H7B3-dk board and already modified the display. I connected a display that supports the DE Sync mode,...
Hello everyone :) I've got some problems with the Scrollable Container. I created a small application based on the "Scrollable Container example". If I scroll the text, there are some issues. There is a delay between scrolling and the updated display...
Hello everyone,I encountered a problem while modifiying the STM32F746G-Discovery board.I modified it like this: switched the 4.3" display to a 5" display (24 bit RGB--> RGB888, 800x480)modified the LTDC settings to match the new display (Can there b...
Kudos given to