cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to configurate the LTDC to Data Enable Mode?

MWetter
Associate III

Hello everyone,

is it possible to use a display that only supports Data enable mode?

If yes, how to configurate the LTDC for this mode?

I use the STM32H7B3-dk board and already modified the display. I connected a display that supports the DE Sync mode, but I have another display that only supports DE mode.

The LTDC documentation does not help.

Thank you very much

2 REPLIES 2
MM..1
Chief II

I mean LTDC generate normal DE signal. If LCD work only with it you can use it.

Maybe HSYNC VSYNC can help over some NANDs...

MWetter
Associate III

Thank you very much. I will try it out and hopefully it will work :)