User Activity

Hi,We are currently using H745 in our design and we noticed this little excerpt in the bootloader manual (AN2606):" Additional reset needed after power off/on to enable connection to the BL interfaces "It seems that not all resets are equal and the r...
Hi,I'm trying to port my project over to Keil uVision, but I'm having hard time flashing the device. It seems that my target values are incorrect.I'm looking for help to get me at least some basic settings done in the scatter file and what settings t...
Hi,I'm having some issues with setting up the IDE for dual-debugging so I can access both the M7 and M4 core in the same IDE.I'm using STLink V3Set for debugging and GDB (I could not get the OCD setup working at all).I have tried going through the st...
Hi,I've been trying to get the SDMM1 working on a custom board with an eMMC (ISSI 32GB).Are there any working examples from ST that verifies you have actually tested the MMC side of the HAL library to be working? @Imen DAHMEN​ I am able to get the CS...
Hi,I'm attaching a picture of my clock configuration and Logic Analyzer (Saleae Logic Pro 8) so it is easier to see what I'm doing.I have set the SDMMC clock divide factor to 1 in the configuration tab, which should produce a divide factor of 2 in th...