cancel
Showing results for 
Search instead for 
Did you mean: 

"eDesignSuite" of Interleaved PFC Specifications

Kdaeg.6
Associate

Helo,

I have recently bought a STEVAL-IPFC01P1, to evaluate de STNRGPF01 controller.

I want input voltage spec to 90-265VAC at 47-63Hz range

How can I change it?

I'm tried the following way...

1) Interleaved PFC Specifications clock

2) "Mains Wide Range Line -> Neutral" selection

Voltage range 85 / 265

Frequency range 47 / 63

Nominal Voltages 115 / 230

3) "Mains EU Range Line -> Neutral" selection

Voltage range 185 / 265

Frequency range 47 / 53

Nominal Voltages 115

4) "Mains US Range Line -> Neutral" selection

Voltage range 185 / 265 Red, range input error

Frequency range 47 / 63 Red, range input error

Nominal Voltages 115

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Carmelo VICCICA
ST Employee

Hi,

in order to select the desired input ("input voltage spec to 90-265VAC at 47-63Hz range") please follows these steps

1) select "Mains Wide Range Line -> Neutral" selection. The tool will be applied rigth constrains for the input boxes.

2) write in "Voltage range min" 90 as value

In attachment a screenshot for this input specification.

Regards.