I was able to open the MX file if I edited the .ioc file to bump the version numbers. I made the following changes:MxCube.Version=5.2.0 ==> MxCube.Version=5.2.1MxDb.Version=DB.5.0.21 ==> MxDb.Version=DB.5.0.21However, I do not know if this introduces...
I am also having this issue in CubeMX v5.1.0. When I click on the ADC configuration in the left panel, CubeMX freezes. I reinstalled version 5.0.1 and I do not have the problem. I do have the latest version of Java 8 for mac installed, so I am not su...