I confirm there is no dedicated VDDUSB on QFN32 package. Request for update of the drawing in DS has been already created, will be done with next planned revision of the document. Pinout table is correct.Thank you to report this point and sorry for t...
Although U0 is good product to replace L0, there are no plans to stop L0 product - plus there is this 10 years longevity program.However, hearing IoT in the text, I would strongly recommend to move to U0 instead of L0 due to security features embedde...
Currently, product is covering flash size from 16 K to 256 K with many intermediate sizes in the portfolio. There is a discussion about possible extension of this product line but nothing could be committed at this moment.