2021-07-10 10:54 AM
2021-07-10 3:53 PM
10 kOhm is typical, but the pin is floating internally so values far higher than this will work as well without drawing additional current.
2021-07-11 4:35 AM
If working in a high temperature environment, leckage current increase substantial and the 10 kOhm might need reconsideration.
2021-07-11 8:27 AM
How high are we talking about?
2021-07-11 8:27 AM
What values would you suggest?
2021-07-11 8:28 AM
To be one the safe side, look at the max. values in the appropriate datasheet.
2021-07-11 8:32 AM
10 kOhm.
2021-07-11 8:32 AM
How would high temperature cause increased leakage on the BOOT0 pin in this scenario?
2021-07-11 12:30 PM
That's the issue, they are not mentioned in the datasheet for this MCU
2021-07-25 11:03 PM
Okay, I have seen that 100Kohm is also used in some MCU, so will there be any difference when using 10K or 100K?