cancel
Showing results for 
Search instead for 
Did you mean: 

What values of pull-up resistors should be used for the BOOT0 and BOOT1 pins in the STM32WB30CE MCU? They are not mentioned in the datasheet for the MCU.

HAgar.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
TDK
Super User

10 kOhm is typical, but the pin is floating internally so values far higher than this will work as well without drawing additional current.

If you feel a post has answered your question, please click "Accept as Solution".
Uwe Bonnes
Chief

If working in a high temperature environment, leckage current increase substantial and the 10 kOhm might need reconsideration.

How high are we talking about?

What values would you suggest?

Uwe Bonnes
Chief

To be one the safe side, look at the max. values in the appropriate datasheet.

10 kOhm.

If you feel a post has answered your question, please click "Accept as Solution".

How would high temperature cause increased leakage on the BOOT0 pin in this scenario?

If you feel a post has answered your question, please click "Accept as Solution".

That's the issue, they are not mentioned in the datasheet for this MCU

Okay, I have seen that 100Kohm is also used in some MCU, so will there be any difference when using 10K or 100K?