User Activity

Hi all,I am using STM32F303CB microcontroller, connected with a I2C slave which has no CLK stretching support. The I2C bus lines are pulled high with 4k75 ohms resistors and the lines have a serial resistor of 50 ohms (approx.). The schematic looks l...
Hi everyone,I am currently migrating from STM32F303x to STM32G431x microcontroller (48-pin package) and started testing the GPIOs in reset state, without any firmware on-board. Also, there are no external HW circuitries connected to the pins (I meant...
I am currently using the STM32F3 series microcontroller (STM32F303CB) in a magnetic sensing application. Since the environment is prone to magnetic field, I wish to know the maximum field strength that the microcontroller can withstand.I could not fi...
Scenario – Currently I am using STM32F303CBxx as my slave and an Infineon microcontroller as a master. The communication takes place via SPI with the clock frequency as high as 1.985 MHz (approx.). The master and slave are inside a closed metal compa...
Hi everyone,I tried installing the package "BlueNRG GUI 3.1.0" and I faced certain issues during its installation. First one, there was an issue in driver installation. I am using the STEVAL - IDB008V2 board. But the main issue is with the installati...