cancel
Showing results for 
Search instead for 
Did you mean: 

H750VBT6 BKPSRAM can't keep DATA

ZYubi
Associate III

 /* Enable write access to Backup domain */

 PWR->CR1 |= PWR_CR1_DBP;

 while((PWR->CR1 & PWR_CR1_DBP) == RESET)

 {

 }

 /*Enable BKPRAM clock*/

 __HAL_RCC_BKPRAM_CLK_ENABLE();

  

 *(__IO uint32_t*)(0x38800000+36) = 12345678;

run to here, DATA 12345678 is written to adress 0x38800000+36 , but I reset the chip,the DATA in adress 0x38800000+36 has been changed,I don't konw what's the reason?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Check power supply on VBAT pin.

VBAT is OK. I used ​the ADC3 to measure the voltage of VBAT, the value is about 3V.