I perform the following steps:1 Load the board using the board sellector2 On the pinout view activating a PA8 pin and reseting that PIn to its defaults3 Generate code by "save"4 Build the project "Build project"5 Run "Debug AsSTMicroelectronics ST-LI...
STMicroelectronics ST-LINK GDB server. Version 5.8.0Copyright (c) 2020, STMicroelectronics. All rights reserved.Starting server with the following options: Persistent Mode : Disabled Logging Level : 1 Listen Port Number : 6123...
Hai 1-I have orded a new USB kabel and waiting for the delivery. 2-I have installed the Cube program toolI am new to this tool but it did not connect well, I do now beter understand the toolWhat I see in the log is a DEV_CONNECT_ERRI have updated the...
Hai I still have this problem with the debugger. I am using Windows 10 and did a complete new installation of the STM32CubeIDE software but the problem with the debugger is still there. I installed the development board STM32L476RG activated 1 extra ...