cancel
Showing results for 
Search instead for 
Did you mean: 

I have init a new project and try to run it. I follow the you tube video. The debugger is stopping and I recieve an error Waiting for debugger connection... Debugger connected Debugger connection lost. Shutting down... Need help getting started

JNiva.1
Associate II

STMicroelectronics ST-LINK GDB server. Version 5.8.0

Copyright (c) 2020, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Waiting for debugger connection...

Debugger connected

Debugger connection lost.

Shutting down...

Software update is returning errors:

An error occurred while collecting items to be installed

session context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).

No repository found containing: osgi.bundle,com.st.stm32cube.common.mx,6.2.1.202103241236

No repository found containing: osgi.bundle,com.st.stm32cube.common.mx.oss,6.2.1.202103241236

No repository found containing: osgi.bundle,com.st.stm32cube.common.mx.stinsider,6.2.1.202103241236

No repository found containing: osgi.bundle,com.st.stm32cube.common.projectcreation,1.6.1.202103171520

No repository found containing: osgi.bundle,com.st.stm32cube.ide.documentation,1.6.1.202103260948

No repository found containing: osgi.bundle,com.st.stm32cube.ide.mcu.ide,1.6.1.202103171520

No repository found containing: osgi.bundle,com.st.stm32cube.ide.mcu.rcp,1.6.1.202103171520

No repository found containing: osgi.bundle,com.st.stm32cube.ide.mpu.linux.ide,1.6.1.202103261436

No repository found containing: org.eclipse.update.feature,com.st.stm32cube.common.feature.mx,6.2.1.202103241236

No repository found containing: org.eclipse.update.feature,com.st.stm32cube.common.feature.mx.stinsider,6.2.1.202103241236

No repository found containing: org.eclipse.update.feature,com.st.stm32cube.common.feature.projectcreation,1.6.1.202103171520

No repository found containing: org.eclipse.update.feature,com.st.stm32cube.ide.feature.documentation,1.6.1.202103260948

No repository found containing: org.eclipse.update.feature,com.st.stm32cube.ide.feature.mcu.ide,1.6.1.202103171520

No repository found containing: org.eclipse.update.feature,com.st.stm32cube.ide.feature.mcu.rcp,1.6.1.202103171520

No repository found containing: org.eclipse.update.feature,com.st.stm32cube.ide.feature.mpu.linux.ide,1.6.1.202103261436

No repository found containing: org.eclipse.update.feature,com.st.stm32cube.ide.feature.mpu.linux.projectcreation,1.6.1.202103261436

No repository found containing: org.eclipse.update.feature,com.st.stm32cube.ide.feature.mpu.linux.toolchain,1.6.1.202103261436

No repository found containing: binary,com.st.stm32cube.ide.mcu.rcp.product.executable.win32.win32.x86_64,1.6.1

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
JNiva.1
Associate II

Hai I still have this problem with the debugger. I am using Windows 10 and did a complete new installation of the STM32CubeIDE software but the problem with the debugger is still there.

I installed the development board STM32L476RG activated 1 extra GIO IO pin and generate code

Build project

10:40:08 **** Incremental Build of configuration Debug for project 9Dof ****

make -j4 all 

etc

Finished building target: 9Dof.elf

arm-none-eabi-objdump -h -S 9Dof.elf > "9Dof.list"

arm-none-eabi-objcopy -O binary 9Dof.elf "9Dof.bin"

arm-none-eabi-size  9Dof.elf 

  text   data   bss   dec   hex filename

 12036    20   1700  13756   35bc 9Dof.elf

Finished building: default.size.stdout

Finished building: 9Dof.bin

Finished building: 9Dof.list

10:40:12 Build Finished. 0 errors, 0 warnings. (took 4s.531ms)

STMicroelectronics ST-LINK GDB server. Version 5.8.0

Copyright (c) 2020, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Waiting for debugger connection...

Debugger connected

Debugger connection lost.

Shutting down...