User Activity

When I tried to open my existing project for the first time in CubeMX 5.5.0, it gives me a pop up window (See attached)But I can't click the link that is refered in the window "Stm32cubemx_gfx_mw_migration) note.
I started a project from scratch in CubeMX. and the set TouchGFX for portrait as :Middleware->Graphics->TouchGFX, changed width : 272 and Height : 480. In TouchGFX designer it displays correctly as Portrait(see PortraitFromTouchGFX).PNG) but when I c...
1)     Created a sample project using CubeMX(5.0.0), TouchGFX(4.10.0) for STM32F46G-Disco board2)     TouchGFX GUI : is very simple just three buttons, and a background image – Code generation was OK, No Error3)     Generated the code from CubeMX for...
Kudos from