User Activity

Hi, I'm very disappointed using STM32CubeIDE v 1.7.0When I go into "Debug" there are no ways to see the variables, both tabs Live Expression and Expression.I would like debug my project (fp_cld-azure with several custom source adds ) but I'n not able...
Here below image of the MCU on my two nucleo boards. I tried to program the MCUs using SMT32CubeProgrammer and USB-TTL converter connected to USART1 via pin PA9 and PA10, BOOT pin tied to 3V3. I press the reset button, then try to connect F070 MCU bu...
Hi, I'm using a Discovery IoT Board B-L475E-IOT01 with application FW STM32CubeExpansion_Cloud_AWS_V1.2.0. I test the application with my think registered on AWS on september, that use the following endpoint ULR: a8yx4uphexpln.iot.eu-west-2.amazonaws...