User Activity

I have installed STM32CubeIDE 1.6.1 on a Windows 10 client. I want to load firmware examples, which I already have stored on the machine. The IDE will not connect to the network. It continually prompts me to connect to the network, but when I clic...
I'm trying to write code for an SNTP clock using the UTIL_LCD routines in the STM32H735G-DK firmware. I'm using lwIP and FreeRTOS for my implementation. I have the clock working with the LCD_TRACE display (the logging display that is used by the web...
I have an STM32H735G Discovery Kit and I'm using it with STM32CubeH7 IDE.I want to modify the projects for my own code. Specifically, I want to make a copy of a project.But, I MUST keep the metadata for the toolchain and the debugger. Right now, I ...
Specifically, I'm looking for the minimum board configuration that will run in STM32CubeIDE, and an explanation of what the minimum settings are and in which memory space the firmware runs in. Is there a project in the STM32 library that uncondition...
I have a STM32H735-DK and I'm trying to load the LedToggling sample app with the STM32CubeIDE 1.5.1. Debug fails with this message.Starting server with the following options: Persistent Mode : Disabled LogFile Name ...
Kudos from