Thanks Khouloud,I don't need any actual audio record/playback.Would the FatFs_uSD_Standalone example allow me to load files via uSD card port?. This runs on the cheaper STM32H735G-DK board so would be better.Cliff
Thanks for the response Khouloud,Let me clarify what I want to do so that you can make a suggestion:I have a audio codec application that takes a .wav and writes a compressed file. It's written and optimized for Cortex M7 (STH750B) and I want to make...
That's disappointing. Maybe should have picked a different board? printf() is a wbni but getting a test file in and a test file out of the board is a must to validate the implementation and measure performance. I could obviously put the input test da...