Hello,STWBC2-HP continues, but STWLC99 is stopped.For Rx part, STWLC38 is available (up to 15W) and a new product should be released this year up to 30W.For Tx, STWBC86 can deliver up 5W and STWBC2-HP covers the whole range (even up to 100W).BR,Didie...
Dear customer,ST has decided to reduce its portfolio to the most successful devices.Unfortunately, STWLC98 is not part of this portfolio and it is going to be stopped.Sorry for the inconvenience,Didier H.
Hello,You can pulled up these pins (SDA and SCL) up to 6V (4.5V max would be better as a steady state), it will not impact the chipset.Nevertheless, if the STUSB4500 is not supplied (no charger connected), be aware that you will get a leakage current...
As an alternative to the original coil, you can look for a coil which is compliant to MP-A11 profile, defined by the Qi standard. It should allow you to charge off-the-shelf receivers up to 5W with the STWBC86 platform. The MPA11 has been defined as ...
Sorry, but I can not review you code.You will find a code example to access to the STPM32 on st.com: https://www.st.com/en/embedded-software/stsw-stpm002.htmlYou will get a 5 bytes answer after your reading request: bit [0:14] is the RMS voltage, bit...