cancel
Showing results for 
Search instead for 
Did you mean: 

BLE Mesh on BlueNRG-1 w/Proxies?

TJohn.14
Associate II

I have an existing phone app (using the traditional GATT system), and I would like mesh-enable my products so that if the products can see each other, then the phone can connect to and control any node (so, not so much an automation system but a relay system for configuration messages).

1. Is there a good tutorial on how the mesh-proxy connection works in the firmware/phone side (does the proxy "broadcast" all the BLE Node addresses so it's truly transparent, or should I put in a GATT attribute for "I really want to connect with  this node?" or?

... I understand how the pieces are relayed over-the-air, but I'm not sure how to configure the stack and the phone app.

2. Can I pre-share the Network Security Key for a "all nodes are part of the mesh out of the box"? I don't expect the factories that our sensors are in to be close to each other (and if they are, cutting nodes out would be just as easy as commissioning them in...

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0