User Activity

Dear Sir/Madam,It seems that DMA2D_OPFCCR register SB bit described in the reference manual of the the STM32H7 (RM0433, page 721) is not implemented. Code generated by CubeMX is missing the definition completely, an attempt to set the bit directly fr...
Posted on July 13, 2018 at 08:56Dear Community,Is there a place that we can contact the developers of HAL in a more formal manner than this forum?Any how, I see that HAL provides separate date and time functions to set and get the date and time:- HA...
Posted on July 11, 2018 at 10:15Dear Community,I am new to the STM32, have used the Renesas platform in the past, it seems to me that the STM32 HAL is using precious (S)RAM memory for information that could be considered constant.For each peripheral...
Posted on July 11, 2018 at 08:38Dear Community,Reading the datasheet and reference manual of the STM32H7 I am left wondering whether if it is possible to have both the DRAM and NOR/SRAM controllers of the FMC controller active at the same time?The m...
Kudos from