Hi Decemberman, There isn't a script to erase a specific block memory yet, but you could use this one as an example: spc582b_dis_FLASH_ERASE_ALL.cfg. you can find this file under C:\AutoDevKitStudio-2.4.0\openocd\scripts\utility. Read the readme.txt ...
Hi Aishwarya UMThe FDA903D audio amplifier provides the ability to detect the open load even in play.If the audio signal is judged to be good enough to provide a reliable result, the test result is valid. Otherwise, if the audio signal doesn't allow ...
Hi Shiva_ShankarThe FDA903D audio amplifier provides the ability to detect the open load even in play.If the audio signal is judged to be good enough to provide a reliable result, the test result is valid. Otherwise, if the audio signal doesn't allow...
Hello Decemberdream,the pin modes indicate the direction of the signal depending on the micro, i.e. mode_input means that this pin is set as the input pin of the micro, pin_output means that this is a pin from which the signal goes out of the micro. ...