Yes, there are two ways how to address more than one sensorUse different I2C buses of the MCUUse I2C switch. For example TCA9545A. I'm using the second way to address 12 sensors in my device
Hello, JohnSimilar question just with different return result..I'm also using ULD driver with default settings in the VL51L1X_DEFAULT_CONFIGURATION array. My sensors work fine when there is some obstruction on the working distance (up to 3.5-3.9 mete...