User Activity

Hello,what is the difference between configuring GPIO pins from software and leave as default(no code). does it have an impact on other register settings that are not being set/clear in default configuration. because I am having a problem when I leav...
Hello,I would like to know, why unconfigured pin is consuming power when it is connected to 3.3 volt, while it is in analog input mode (reset mode as per to the data sheet). here, what i have tested with three configurations.with pin configuration(PA...
Hello,After access to board selector > STM32F446RE does not ask for the default peripheral configuration and it started as a plan board.What can be the reason not initialization of the default pin of the board?Thanks.
Hello, I am using STM32F100CBT6B in my project and I am in need of having one more UART port and I came across following example folder STSW-STM32156. Please let me know if it is possible to instrument this file to the F1 Series. Thank you.