2019-11-02 2:04 PM
Hi,
I would like to use the STUSB4500 USB-C PD AutoSink board replacing the big power supply to
power up the motor drive board IHM02A1 which would require at least 8 volt. But the motors can not move and I found out the output from the STUSB4500 board is only 5 volt after I connected them together. Isn't that the STUSB4500 pre-configured with the 15V/20V profiles? Do I need to do anything to bring up the voltage?
Thanks in advance.
Duncan
2019-12-05 5:39 PM
Hello,
In the STUSB4500 datasheet, the initial setting is shown in "Table 16. STUSB4500 user-defined parameters and default settings"
So STUSB4500 default PDOs settings are: 5V/1.5A, 15V/1.5A, 20V/1.0A
After connecting the USB-C cable, if the output on VBUS is 5V, it means that the USB-C Power source cannot provide 15V or 20V.
- So you'll need to use a different Power Source which can provide the 15V profile.
- Or you'll need to reprogram the STUSB4500 with lower profiles (e.g. 5V, 9V, and 15V)
To know which USB-C power source can provide 15V, you need to use a power supply labeled with at least 45W.
The supported output voltages are generally written on the power supply itself.
Best regards.