User Activity

We have encountered a problem with CRYPTO IP core on STM32MP157C.Our setup is STM32MP157C-DK2 with latest image/SDK installed(openstlinux-5.10-dunfell-mp1-21-11-17).1. First of all, our IPSec solution based on strongSwan doesn't work atall when stm32...
Hi,I'd like to be able to read/write for debug purposes peripheral registers of the MPU and MCU from Linux user space. Of course all under root permissions. The most straightforward way should be doing it using /dev/mem but I'm not sure if it is a be...
Hello.I have a STM32 Nucleo board and a USB dongle. What Stack and FW should be programmed to use STM32CubeMonitor-RF 802.15.4 RF test mode described in chapter 5 of the UM2288?Thanks.
Hello, after playing a bit with P-NUCLEO-WB55 pack I bricked the board.The board is visible by Cube Programmer in DFU mode. Programmer can see the ST-Link but ST-Link does not detect the target. Are there any suggestions to recover ST-Link connection...
Hello.I have a task to evaluate RF range and penetration of the STM32WB based module. We plan to migrate from Microchip module to STM32WB5MMG module. The +6dBm output power of the ST module is a bit concerning compared to +20dBm we had from Microchip...