2021-03-03 6:44 AM
Hello.
I have a task to evaluate RF range and penetration of the STM32WB based module. We plan to migrate from Microchip module to STM32WB5MMG module.
The +6dBm output power of the ST module is a bit concerning compared to +20dBm we had from Microchip.
What is the best way to make an evaluation and field testing using P-NUCLEO-WB55
pack ?
I have installed all the STM32WB ecosystem and even managed to brick one of the Nucleo boards. But still have one board and two USB dongles operating.
Thanks.
2021-03-29 8:37 AM
I'm back to evaluation. Can anyone please help me pointing to the right way to do it?
How can I take P-NUCLEO-WB55 Board and Dongle and make a communication test between these devices?
Thanks.
2021-04-01 9:11 AM
OK.
I have found a CubeMonitor-RF presentation that explains how to run PER test on BLE devices.
Presentation also states that it is possible to run PER test on 802.15.4 devices.
For BLE case there is a BLE_TransparentMode FW application. What should I do for 802.15.4 case? What Stack and what FW should be run?
Thanks.