User Activity

Questions:1. When do I use FSM and when do I use Decision Trees? Can I use both?2. Do you call ML the use of decision trees and NOT FSM?3. What I want is to detect gestures like if the sensor was in a pen and I wrote letters, let's say E, M, V, etc. ...
Hi,I need to be able to change "BOOT_ADD0" and the following code doesn't work; please help.For one thing I have no idea if it's FLASH_BANK_1 or 2 that I'm interested in.Then I'm hoping that "...GetConfig" populates everything and I only need to chan...
Posted on August 14, 2017 at 23:13I need help setting up and enabling (and disabling) the  Spread Spectrum Clock on STM32F405.AN4850 is not enough, as it has no code example; says nothing about what to do with MODPER and INCSTEP once calculated.I se...
Posted on September 23, 2015 at 21:53I have this SPL project on STM32F427 that I need to migrate to STM32F746. I was hoping I can just program the F7 and it will run but that just shows how naive I am :) Anyway, I wish there was an SPL for the F7 so...
Kudos from