2018-08-20 1:01 PM
Hi,
I need to be able to change "BOOT_ADD0" and the following code doesn't work; please help.
For one thing I have no idea if it's FLASH_BANK_1 or 2 that I'm interested in.
Then I'm hoping that "...GetConfig" populates everything and I only need to change a few things but I'm not sure.
Help, please?
Thanks,
Cat
HAL_FLASH_OB_Unlock();
HAL_FLASH_OB_Launch();
FLASH_OBProgramInitTypeDef Cats_pOBInit;
Cats_pOBInit.Banks = FLASH_BANK_1; //Which one?
HAL_FLASHEx_OBGetConfig(&Cats_pOBInit);
Cats_pOBInit.OptionType = OPTIONBYTE_BOOTADD;
Cats_pOBInit.BootAddr0 = 0x1FF0;
Cats_pOBInit.OptionType |= OPTIONBYTE_WRP;
Cats_pOBInit.WRPState &= ~OB_WRPSTATE_ENABLE;
HAL_FLASHEx_OBProgram(&Cats_pOBInit);
HAL_FLASH_OB_Lock();
2018-08-20 1:49 PM
Note: The "-" in front of "OB_WRPSTATE_ENABLE" is in fact a Tilde. I don't know how to make it look like one.
2018-08-23 1:55 PM
I think I got it.
The following seems to work but I think not everything I have here is needed:
FLASH_OBProgramInitTypeDef Cats_OBInit;
HAL_FLASH_Unlock();
HAL_FLASH_OB_Unlock();
HAL_FLASHEx_OBGetConfig(&Cats_OBInit);
Cats_OBInit.Banks = FLASH_BANK_1;
Cats_OBInit.OptionType = OPTIONBYTE_BOOTADD;
Cats_OBInit.BootAddr0 = 0x1FF00000;
Cats_OBInit.BootConfig = OB_BOOT_ADD0; //Specifies Boot Address to be configured: must be OB_BOOT_ADD0, OB_BOOT_ADD1, OB_BOOT_ADD_BOTH
HAL_FLASHEx_OBProgram(&Cats_OBInit);
HAL_FLASH_OB_Launch();
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.