i am using touchGFX designer V4.18.0. In software run target option is disabled.how can i recover that so please tell me the process to get run target option.
Hi , I am working on STM32F469I-DISCO kit.In that actually Internal RTC time is not runningI configured internal rtc from cubemx. I am getting Time what i did set time only.no more time is running. support me what the issue for not running time.
I am working on touchgfx LCD. I need a a support to develop our custom application.i have seen touchgfx API functions setup screen but i need example for better understanding.
hi,I told you my previous issue. No can solve still can you please check my problem. Core/Src/main.c:24:10: fatal error: usb_device.h: No such file or directory #include "usb_device.h" ^~~~~~~~~~~~~~ compilation terminated. gcc/Mak...
Actually i am using STM32F469I-Disco kit . when i add usb virtual com port in cubemx i got compile error in touchGFX but no error in stmcubeide.at that time based on Community member instructions I did the below process.took a stmcubemx .ioc file fro...
hi,ok can i copy that cmds from old project?i got this error making run targetCompile make -f ../gcc/Makefile -j10 make: ../gcc/Makefile: No such file or directory make: *** No rule to make target '../gcc/Makefile'. Stop. Failed Failed
what ? that is not a cause.. If i opened directly from touchGFX designer that run target option came in active.I did the below process.took a stmcubemx .ioc file from my old project because of some usb related errors in touchGFX.Copy that file in to ...