User Activity

Hello,Some requests for support.History:Motor profile generated for I-PMSM motor.Motor profile carried out with:NUCLEO-F303RESTEVAL-IPM20BSee attachment (JEE15IHM1150012MH.zip) for motor profile result.After this MC workbench project made with invert...
We want to use the HSE clock for above mcu. To whicjh pins do we connect the osc?We are missing the osc_out pin?
See AN436. I am using T1635-6G in a Hybrid Relay configuration following AN4993. Load is about 2kW at 230 VAC. Circuit works fine at with gate traiin of pulses (2kHz, DC = 50%). I want to trim parameters to optimum, at the moment transformer is make ...
Quote from page 11:The M0-7 standard high-side drivers are manufactured using STMicroelectronics® proprietary VIPower® technology. The devices are designed to drive 12 V automotive resistive as well as inductive and capacitive loads connected to grou...
Kudos given to