Posted on August 21, 2017 at 18:12Subj.The problem is an ''Option bytes'' dialog form is too ''tall'' and I can't do it smaller. My screen resolution is 3200*1800 and even I hide Task Panel I don't see a form's bottom.
Posted on August 19, 2017 at 20:48An ST-Link (from Nucleo-64) don't want to read an STM32F030RCT6 under Windows 10 (64 bit) with a message 'Can not connect to the target'. The most interesting thing is it reads an another same board already programm...
Posted on August 02, 2015 at 17:47 What does these 3 parameters mean? RM0360(''STM32F030x4/x6/x8 advanced ARM-based 32-bit MCUs'') tells nothing about the possibility of use a binary format. Also, daylight saving is only the possibility to add ...
Posted on July 16, 2015 at 12:41Who can tell me, how to change processor already selected? If I've found that the selected became too small for my firmware? I would like to change it for the bigger one with compartible pins. #stm32cubemx
Posted on August 21, 2017 at 17:54I've checked signals with an oscilloscope. It seems a port responsible for NRST signal is burned out. Sometimes access to an MCU is successful, sometimes not, but a shape of the NRST is far from normal. By the way, ...
Posted on August 20, 2017 at 01:01I used one ST-Link and board on both computers. And, of course, I've updated everything I could update. I've tried to connect under reset and all other possible modes. And only after that, I wrote the previous messa...