When build the project, the ide generate the bin file and include large mount of zero at the end of the file. I try to set the ram2's load address to solve this problem.Isthere any other way?
When build the project, the ide generate the bin file and include large mount of zero at the end of the file. I try to set the ram2's load address to solve this problem.Is there any other way?