User Activity

Hello, I'm working on STM32G0B1KET6N uc with custom board.When I'm using this tutorial: https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Sink everything is working great, my device is acting as USB PD Sink. Bu...
Hello,I am working on the STM32G0B1RE processor as a USB-PD SINK.I would like to ask what is the easiest and fastest method (preferably using CubeMX) to request higher voltages from the USB-PD port (for example 9V or 12V)? Can anyone share the simple...
Hi, I have few of this Nucleo boards (-F103RB, -F072RB, -F401 etc.). I would like to use ST-LINK VCP to communicate with MCU over the USART2 but I cannot find any information about parameters of this communication (I mean baud rate, parity bits etc.)...