cancel
Showing results for 
Search instead for 
Did you mean: 

Is U-boot support for STM32MP157F-DK2 planned any time soon ?

SThon.1
Associate II

Hi,

I can currently only find support for STM32MP157A-DK1 and STM32MP157C-DK2 boards in u-boot.

Is there a plan to support the STM32MP157F-DK2 board in the near future?

Kind regards,

Steinar

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hi,

STM32MP157F-DK2 is supported from day 1 when the board has been released.

https://wiki.st.com/stm32mpu/wiki/STM32MP15_U-Boot#Selecting_targets_-_choose_defconfig_and_device_tree

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here