User Activity

Hi ST_community."Programing STM32F429ZIT6 micro"I have a question: what are the options to burn/download a program into a STM32F429?At this moment, I am working on STM32F429ZIT6-DISC1 board, now, everything is ok, everything is done it throughout ST_...
Hello STM32 Community.I need your support, I am trying to do a small project where I need to use for example a var where PWM frequency is saved, as I need to calculate the period I just write a division 1/test_float and the result must be the period....
Hi all.I am trying to connect 2 STM32F103C8 (blue pill board).I run a test using just ONE STM32 using SPI1 as Master and SPI2 as Slave, all configurations were working fine (FullDuplex, Master Transmite. receive only Slave....every test was fine (all...
Hello everyone.I am working on a project, where It has 6 PWM channels, and there will be 3 channels active at time, As all PWM channels must have the same frecuency, all PWMs channel must start and stop at the same time, I am trying to define TIM2 as...
Hi ST Community.I need your help. I am working on a PWM Proyect, Duty cicle must be change every period, and there is delta time where the PWM must be OFF.I am using a Timer, it fire an interrution and this interruption set a flag to 1 in order to r...
Kudos from