Skip to main content
Nidhal Abidi
Associate II
April 17, 2018
Question

Powering up stm32

  • April 17, 2018
  • 8 replies
  • 3283 views
Posted on April 17, 2018 at 17:43

which is best to power up    ''' STM32VLDISCOVERY '''   via 5V pins and a ground or 3,3V ???

also which is best to for Digital Input for STM32VLDISCOVERY, using 5v or 3,3V ???

In the data sheet I found that bouth of them works. And when I tryed it, bouth works but in the data sheet reset button and pin PA0(user button) are related to 3,3V.

so wich is the best chice for an industrial

project ???
    This topic has been closed for replies.

    8 replies

    Andrew Neil
    Super User
    April 17, 2018
    Posted on April 17, 2018 at 19:07

    What do you mean, 'best' ?

    As you can clearly see from the schematics, the STM32 itself is running from 3V - so the only difference between powering the board from 3V or 5V is whether or not it goes through the regulator first.

    Check the datasheet for details of the '5V tolerant' pins.

    Also check the datasheet for details of the logic thresholds, but I think you'll find this is set by the STM32's supply voltage (3V) - so you gain no advantage from 5V logic levels.

    undestrial

    You mean, 'industrial' ?

    Note that the Discovery boards are supplied by ST as an evaluation tool - they are not intended as final products, and the licence terms specifically prohibit such use.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Nidhal Abidi
    Associate II
    April 18, 2018
    Posted on April 18, 2018 at 11:57

    Thanks, mmm, what if I power up the stm with 5v and then use the stm's 3.3v out as inputs for the switches, or buttons or whatever ???

    Andrew Neil
    Super User
    April 18, 2018
    Posted on April 18, 2018 at 12:21

    Nidhal Abidi wrote:

     what if I power up the stm with 5v

    Have you actually looked at the datasheet for the STM32 chip?

    It tells you what range of voltages can be used to 'power-up' the chip ...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Nidhal Abidi
    Associate II
    April 19, 2018
    Posted on April 19, 2018 at 09:37

    Great thanks.